ADC sampling rate

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC sampling rate

2,709 Views
cyuk
Contributor I

Hi, I tried to follow up on a old question "https://community.nxp.com/thread/437073", but I didn't get any answers, so now I am raising my own thread.

Based on the K24 Kinetis datasheet:

adc_rate.png

I do not understand, how a sample rate of 461.467 ksps is reachable with a ADC clock limited to 12 MHz. Don't you need 34 adc_clks + 5 adc_clks + 5 bus_clks = 39 adc_clks + 5 bus_clks?

Also, I do see sources talking about high clock frequency than 18 MHz (<= 13 bit mode). E.g. in this example for the same K24 Kinetis datasheet:

Untitled.png

Please, would someone tell me how the 461.467 ksps sample rate is reachable and at which ADC clock?

Thanks, Ulrik

0 Kudos
Reply
1 Reply

2,431 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Ulrik,

With the ADC clock=12MHz, I think it should be 12MHz / 27 = 444.444 ksps

16bit ConversionTime.png

This meet the result in Processor Expert:

16bit ConversionTime PE.png

Refer to the phenomenon descripted in"Figure 1. Voltage drops at ADC input during sampling process" of AN4373.

I think you can observe the waveform of ADC conversion rate on your ADC input pin.

Voltage+drops+at+ADC+input+during+sampling+process.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply