ADC issue on MKE06Z128VLD4R

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC issue on MKE06Z128VLD4R

1,287 Views
jwu
Contributor I

I'm having the ADC issue using MKE06Z128VLD4R. Sensing of 4 ADC channels gets incorrect readings, while sensing single channel gets accurate results. I have tried many things and couldn’t work it out.

If I download the same software binary to FRDM KE06 board (with 80 pin micro), it works accurately. I suspect that this is the second hardware defect in KE06 family.

Is this a known issue?

0 Kudos
Reply
1 Reply

1,131 Views
santiago_gonzal
NXP Employee
NXP Employee

Hello John,

If it works in FRDM-KE06, then your final assumption is not correct. The HW inside all KE06 derivatives is the same, only the pin assignment is different.

Regards,

Santiago

0 Kudos
Reply