ADC external reference usage on MKL33

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC external reference usage on MKL33

1,518件の閲覧回数
elliotwhite
Contributor I

In order to reduce power usage I need to turn off the analog part of the circuit, If I have understood the data sheets

for the MKL33P80  correctly the following (outline) diagram should work (I hope).

adc1.png

I assume that the VREFs when configured correctly are effectively connected to the ends of the resistor chain in the SAR, and that when disabled (BJT off) it is ok to have VREFN float upto VDDA.

Any assistance would be greatly appreciated

ラベル(1)
2 返答(返信)

1,440件の閲覧回数
bobpaddock
Senior Contributor IV

Use a PNP to switch on the high side.

Having the A/D biased above 'ground' by the transistor drop will causes offsets.


It is still best to connect the VAdd/VAss lines to non-switched power.

We can not know what goes on inside the chip and the unpowered section could actually increase current consumption from unbiased internal impedance's.


1,440件の閲覧回数
jorge_a_vazquez
NXP Employee
NXP Employee

Hi elliot white

VDDA and VSSA pins should be always connected, even if you are not planning to use analog modules of your MCU. But in Vref, If you are not planning to use any analog circuit of the KL33 (they are off), then there shouldn't be problem if you left this pin floating, but if you try to use ADC for example, with this pin floating, it will cause you problems.

Hope this helps.

Best Regards

Jorge Alcala

0 件の賞賛
返信