ADC accuracy (FRDM K22)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC accuracy (FRDM K22)

4,264件の閲覧回数
anouarraddaoui
Contributor I

Hello,

I am trying to know what are the reasons, that may cause the offset I am getting from my ADC input.

I am using the code that I wrote (project can be downloaded below). Please check the adc.c and VREF.c files.

 

I made the small circuit in the Photo (a simple voltage devider) and measured the voltage with two different multimeters. to check the voltage and then compare it with the the adc results. I am always getting an offset of about 2..5mV above the correct voltage.

 

The ADC0 is configured to 16-bit mode (LSB = 1/ 65535) and the Reference voltage is the internal 1.207 V (also measured with the multimeters). So the error is Delta_Voltage = 1.207V x (300 / 65535) = 5 mV

 

Some other facts to my ADC configuration :

* I am using the maximal bus clock (60Mhz)

* long sample time

* software trigger

* high speed conversion

I disabled the high speed conversion, but this did not cause any improvement.

I followed the steps in the reference manual for the calibration function.

 

Any recommendations are welcomed.

Original Attachment has been moved to: ADC_EPWM_VREF.zip

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,878件の閲覧回数
anouarraddaoui
Contributor I

I am now getting better results compared to what I had before(1mV or less below the the measured voltage).

The reason for that is that I was using a very high ADC Clock speed.

I was using the bus frequency as an input frequency for the ADC.  ==> ADC_CFG1_ADICLK(0)

(without dividing it   :  ADC_CFG1_ADIV(0)  ==> in this way f_ADCK = f_bus = 60 Mhz )

Now I am still the using the bus frequency as an input frequency for the ADC, but I am deviding it by 8 ==> ADC_CFG1_ADICLK(3) . So f_ADCK = f_bus  / 8 = 60 Mhz / 8 = 7.5 Mhz

I fortunately found  this note in the ADC conversion time calculator software saying:

NOTE : for best results 16 Bit resoltion rquires ADC CLOCK to be 10 Mhz or lower.

I do not remember reading this note in the reference manual.

pastedImage_10.png

0 件の賞賛
返信

3,878件の閲覧回数
rastislav_pavlanin
NXP Employee
NXP Employee

Hi anouarraddaoui,

from your schematic it is clear that the VREF output is loaded by R=220+100=320 ohm, considering 1.2V reference, the volatge reference buffer current should be 1.2V/320=3.75mA. Please, check in K22 datasheet (VREF full-range operating behaviors) whether your selected device is able to be loaded with such current. If not (likely), then please increase the resisitors in your divider to follow specification.

regards

R.

0 件の賞賛
返信

3,878件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi anouarraddaoui,

About the ADC CLOCK you can read the datasheet(K22P121M120SF7.pdf), the maximum frequency of 16bit fADCK is 12MHz.

ADC electrical specifications.png

About the ADC accuracy, I recommend you read the AN4373(Cookbook for SAR ADC Measurements):

AN4373.png

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信