ADC Input impedance.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Input impedance.

2,912件の閲覧回数
henrikalexander
Contributor I

Hi,

I'm a HW designer and is about to design a HW including a KEA64 MCU were we gonna do some ADC readings.

I'm trying to find out the input impedance for the ADC but cannot find this data in the data sheets for KEA64. The only thing if find is Hi-Z state but not what Hi-Z is.

The reasing I'm asking is if were are gonna need to buffer the analog input signal or not. Since this is a cost sensetive  project we would like to skip the buffer stage.

And the resolution is not an issue for the input reading.

//Henrik A

ラベル(1)
0 件の賞賛
返信
1 返信

2,160件の閲覧回数
david_diaz
NXP Employee
NXP Employee

Hello Henrik,

I personally measured the resistance of one of the ADC inputs of the KEA02.

The resistance value is about 500 Kohms,  and therefore, the ADC input impedance is HIGH.

Hope this information will be useful for you :smileyhappy:

Have a great day.

0 件の賞賛
返信