ADC Count variation in MKE04

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Count variation in MKE04

2,079件の閲覧回数
prasannanaik
Contributor III

Hi,

    In MKE04Z64VLH4 , I am sampling an ADC channel which has DC voltage at its input. But, ADC count which  I am getting has variations of 30-40 counts between Minimum to Maximum values. Logic which is used here is by triggering ADC at every 625 usec interrupt of PIT timer. 

  I have attached code which is used for sampling the ADC channel and there is no ripple in the power supply section.

Core clock is 40 MHz, Bus clock is 20 MHz and OSCER clock is 8 MHz.

Is it there any way by which this fluctuation can be reduced to 3-4 counts as DC voltage is stable?

Is it anything missing in code which causing this fluctuations in the ADC count?Please let me know.

Thanks and Regards

Prasanna

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,982件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Prasanna Naik,

  Do you check your MKE04 VREFH, and VREFL?

 The reference voltage must be very stable, otherwise it will be influence the ADC convert data.

 If you connect the ADC pin to GND, the same as VREFL, whether it still has 30-40 variations ?

 Please test it on your side.

If you still have question about it, please kindly let me know.

Wish it helps you!

Have a great day,
Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信