ADC Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC Clock

2,472 Views
dsherman
Contributor III

I'm a little puzzled on one thing about the ADC clock.  According to the KE06 data sheet, the conversion clock has to be between 0.4 and 8 MHz for high speed mode.  If I'm using a 24 MHz bus clock, then I must use bus clock/2 as the source, and divide that by 2 to get to 6 MHz.  What if I divide that by 4 to get 3 MHz?  Does it just mean that conversions take longer?

Labels (1)
0 Kudos
Reply
1 Reply

2,282 Views
daweiyou
NXP Employee
NXP Employee

Hi:

Yes, normally slower ADC clock will take longer time to finish conversions.

24.4.4.5 Sample time and total conversion time

The total conversion time depends on the sample time (as determined by

ADC_SC3[ADLSMP]), the MCU bus frequency, the conversion mode (8-bit, 10-bit or

12-bit), and the frequency of the conversion clock (fADCK).

Dawei You(尤大为)

Mobile: +86 13675169919

0 Kudos
Reply