ACIM Motor identify without blocking (KMS & HVP-MC3PH)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ACIM Motor identify without blocking (KMS & HVP-MC3PH)

1,631 Views
roberto_foelix
Contributor II

I have a closed vibration motor with the following information:
2 pole ACI-Motor
Rated voltage 230VAC
Rated current 2.7A
Nominal frequency 200Hz
Centrifugal force 4.517N

I am unable to block the motor to determine the engine parameters with the Kinetis Motor Suite and HV-Kit.
How can I determine the parameters?

My test facility:

HVP-MC3PH-Kit (High-Voltage Development Platform|NXP ) & HVP-KV46F150M

I did the following measurement with a test motor (3GAA071312-ASE) and the vibration motor.
Once with a frequency converter (Invertek P2) and once with the HV kit & KMS.

 

 

Test-Motor

 

 

Vibration-Motor

 

Motor Pole

 

2

 

 

2

 

Motor Rated Voltage

 

230 V

 

 

230 V

 

Motor Rated Power

 

0.55 kW

 

 

 

 

Motor Rated Current

 

2.2 A

 

 

2.7 A

 

Motor Rated Speed

 

2790 rpm

 

 

12000 rpm

 

Motor Centrifugal force

 

1.88 Nm

 

 

4.517 Nm

 

 

 

FU (Invertek P2)

NXP-KMS (HVP)

 

FU (Invertek P2)

NXP-KMS (HVP)

Effective Switching Frequency

 

16 kHz

? kHz

 

16 kHz

? kHz

 

 

FU (Invertek P2)

NXP-KMS (HVP)

 

FU (Invertek P2)

NXP-KMS (HVP)

Motor Stator Resistance (Rs)

 

8.459 Ohm

3.705 Ohm

 

11.238 Ohm

? Ohm

Motor Rotor Resistance (Rr)

 

5.071 Ohm

3.847 Ohm

 

6.738 Ohm

? Ohm

Motor Stator Inductance (Id)

 

0.3177 H

0.3725 H

 

0.0763 H

? H

Mutual Inductance

 

 

0.3570 H

 

 

? H

Motor Magnetising Current

 

1.2 A

 

 

1.1 A

 

Motor Leakage Coefficient

 

0.114

 

 

0.096

 

Thank you for your support

Roberto

0 Kudos
Reply
1 Reply

1,496 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Roberto,

We have an application note AN4642.pdf, which focuses on the PMSM, as you know that the ACIM parameters measurement is more complicated than PMSM. Generally, you can measure the rotor parameters of ACIM with the

rotor blocked and non-load methods.

https://www.nxp.com/docs/en/application-note/AN4642.pdf

I do not think we have application note for ACIM parameters measurement, anyway, you can submit a question on the "motor control and smart Energy" forum so that the expert on motor control can answer you. BTW, I do not know whether MCAT tools can support ACIM.

https://community.nxp.com/community/kinetis/motor-control-and-smart-energy 

BR

XiangJun Rong

0 Kudos
Reply