AC to DC Converter using MK60DN512VMD10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AC to DC Converter using MK60DN512VMD10

1,300 次查看
nbjasani
Contributor III

Hi,

 

   We are now working with MK60DN512VMD10 Device. I need to configure this device for 6 Pulse Thyrister converter and H-Bridge IGBT Inverter control logic. So my question is, which timer use for 6 Pulse Thyrister converter and H-Bridge PWM IGBT Inverter?

 

  Is any document which can guide for configuring this device for 6 Pulse Thyrister firing for AC to DC Converter?

 

Thanks

Nandish Jasani.

2 回复数

1,252 次查看
FelipeGarcia
NXP Employee
NXP Employee

Hi Nandish,

 

You can accomplish this by using 6 PWM signals. MK60DN512VMD10 has three FlexTimers with 12 channels. If you need sample code you can download our SDK from the below link.

Welcome | MCUXpresso SDK Builder

 

In addition, please refer to the following application note that explains in detail FTM functionality.

https://www.nxp.com/docs/en/application-note/AN5142.pdf

 

I hope it helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,252 次查看
nbjasani
Contributor III

Hi Felipe

    Sorry for the late reply. Yes i read AN5142 app note and its useful. Thanks for your help.

WBR

Nandish