A project used keil5

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A project used keil5

1,521件の閲覧回数
254218026
Contributor I

Need a complete sample project using KEA128 Micro Controller. IDE used is KEIL.

ラベル(2)
0 件の賞賛
返信
1 返信

1,454件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

Unfortunately there is no MCUXpresso SDK support for KEA series.
It's my understanding that KEA support is moving into the S32 family. As you may know, we've created a completely separate set of tools for S32 (S32DS, for example) and it will support all automotive devices including ARM based chips like KEA and S32 with M4.

 

Please download the S32DS-ARM: S32 Design Studio IDE for Arm based MCUs(S32-DS-ARM_v2018-R1)


You can refer the examples in FRDM-KEA Quick start package (REV 8 ), it can be found at FRDM-KEAZ128: KEA Freedom Evaluation Board

Jianyu: 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信