9 bit dma uart RS485

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,623件の閲覧回数
albertomainoni
Contributor I

Please, how can I get and send ninth bit with DMA and UART?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,279件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

It will be better to use software to set/read UARTx_C3 [T8] about 9-bit UART transmit/receive.

Even if using the DMA engineer, it also need core intervene to write/read the ninth data bit with UARTx_C3 [T8] bit.

Wish it helps.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,280件の閲覧回数
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

It will be better to use software to set/read UARTx_C3 [T8] about 9-bit UART transmit/receive.

Even if using the DMA engineer, it also need core intervene to write/read the ninth data bit with UARTx_C3 [T8] bit.

Wish it helps.

0 件の賞賛
返信