7 " LCD interfacing with ssd1963

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

7 " LCD interfacing with ssd1963

1,262 Views
mayurkhandagale
Contributor I

Hello Sir,

I have KD20070 7" LCD with controller ssd1963.

how i interface with KD60 controller?..in KDS 3.0.0 IDE.

what write(), read() init() command i write?/

can you please guide me to display on screen...!!

reply soon Thank You!!

0 Kudos
Reply
1 Reply

1,153 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Mayur,

I do not find the KD60 in Freescale home page, do you mean the Kinetis family MK60? if it is the case, I think you can use FlexBus of MK60 to interface with the ssd1963, the FlexBus is a memory interface.

Hope it can help you.

BR

XiangJun Rong

0 Kudos
Reply