5v Tolerant pins as Open Collector Drivers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

5v Tolerant pins as Open Collector Drivers

ソリューションへジャンプ
6,001件の閲覧回数
myke_predko
Senior Contributor III

As I was reviewing the datasheets/reference manuals of the MK21FX512VMD12 and MK22FN1M0AVMD12, I noticed that there was the comment that all GPIO pins are 5V tolerant.  

Going through the questions about this previously, it seems that only the input functionality of the pins are 5V tolerant, the outputs (even if they are in open drain mode) engage the anti-static diodes to the chip's Vdd and are only tolerant to what Vdd which is a maximum of 3.6V.  

In my application, I have a number of pins that are driving NPN transistors as open collectors drivers to 5V circuitry and I was wondering:

Could I use the pins as 5V open drain outputs if, when the driver is disabled the pin is in input mode (and is 5V tolerant) and when I want to pull the line low (which the NPN transistor was doing) change to output mode with a low output?  

It's certainly no less kludgy than using the NPN transistor, and it saves me $0.05 in each instance.  

Thanx!

0 件の賞賛
返信
1 解決策
5,988件の閲覧回数
bobpaddock
Senior Contributor III

If get rid of the transistors watch the total package sink current that is allowable on Vss.
Getting close to that can cause ground bounce problems during load switching, if many outputs transition at the same time.

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
9 返答(返信)
5,989件の閲覧回数
bobpaddock
Senior Contributor III

If get rid of the transistors watch the total package sink current that is allowable on Vss.
Getting close to that can cause ground bounce problems during load switching, if many outputs transition at the same time.

 

 

 

0 件の賞賛
返信
5,976件の閲覧回数
myke_predko
Senior Contributor III

@bobpaddock 

In one case the pins are driving the inputs to a TC74AC138FTEL (CMOS Logic) with an equivalant input of:

74AC Input Circuit.jpg

So I think I can use a 100k for the pull up.  

In the other case, it's five PNP transistors (MMBTA06LT1G - Hfe of 100) of which only one should be active at any time that will need a maximum of 200mA through it, which means I should be drawing 2mA through it.   

When I do a power inventory, according to the Datasheet, Idd_run (Run mode current - all peripheral clocs enabled, code executing from flash) = 49.9mA (I obviously use 50mA for my calculations).  The current application circuit's peripheral total worst case (which shouldn't happen) current sink from all peripherals active = 103mA.  The maximum current draw for normal operation is 84mA.  Remove the NPN transistors will drop the worst possible case number to 86mA and the normal operation maximum current sink to 66mA.  It also provides me with a cost reduction of about $0.45 per PCB.  

Idd (Total sink current for the device) = 185mA so in any case I'm not exceeding the total sink for the device so I think I'm good.  

0 件の賞賛
返信
5,973件の閲覧回数
bobpaddock
Senior Contributor III

Yes current sounds reasonable.
185mA in a small package does fell a bit toasty.

Alas those static protection diodes are there for a reason.  It is not clear to me if you are saying you are using the series without the protection diode to Vcc?  
It becomes more of a board handling issue, physically, than run time issue.
Presumably all the normal anti-static precautions are taken to make that a non-issue.

0 件の賞賛
返信
5,969件の閲覧回数
myke_predko
Senior Contributor III

@bobpaddock 

185mA at 3.3V is 0.61W in this package shouldn't get that "toasty", you're talking 169 mm^2 in area with a large Gnd and 3V3 Plans for heat dissipation - I haven't noticed any real increase in heat around the MCU (and I have been checking it with a thermal imaging camera).  

I'm not sure what you mean by "you are using the series without the protection diode to Vcc" - as I understand it (and it seems to be confirmed in multiple posts to this forum) that in the Kinetis, digital pins (not analog) in input mode do not have an ESD diode to Vdd.  The datasheets have the note:

5V Tolerant Pins.jpg

Again, it appears this is the case when the pin is in input mode but not any of the output modes (in those cases there is diode protection to Vdd).  

So, the plan is to keep the IO pin in input mode until I need to sink current, at which point I will change the pin to an output (driving a low value).  With a current limiting resistor, this should properly simulate an open collector output

0 件の賞賛
返信
5,965件の閲覧回数
bobpaddock
Senior Contributor III

I was referring to the Figure 1.2 for the VHC.

 

 

 

0 件の賞賛
返信
5,961件の閲覧回数
myke_predko
Senior Contributor III

@bobpaddock 

Sorry?  I don't know what "VHC" is and none of the NXP documents have a Figure 1.2.  

0 件の賞賛
返信
5,951件の閲覧回数
bobpaddock
Senior Contributor III

I am refereeing to the TC74AC138FTEL image posted above, not the NXP part.
VHC without static diode to Vcc is on right.

 

 

0 件の賞賛
返信
5,941件の閲覧回数
myke_predko
Senior Contributor III

Hey @bobpaddock 

I modified a prototype PCB by taking out the NPN transistors as detailed here and things worked as expected.  

0 件の賞賛
返信
5,947件の閲覧回数
myke_predko
Senior Contributor III

@bobpaddock 

Sorry, I should have looked there - I had moved on from the demuxer.  

I'm using the TC74AC138FTEL (the left side of Figure 1.2), not the VHC.  The AC has the ESD diodes in the input so there shouldn't be any worries.

0 件の賞賛
返信