5.0 Beta stack: Dead and RNDIS-specific code in usb_cdc.c

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

5.0 Beta stack: Dead and RNDIS-specific code in usb_cdc.c

2,279 次查看
johnstrohm
Contributor III

In file usb_cdc.c, lines 406-410 are as follows:

        /* Get count of endpoints for a specific configuration */

        USB_Cdc_Get_Desc_Info(cdc_obj_ptr, USB_CDC_EP_COUNT, &ep_count);

        /* Get count of interfaces for a specific configuration */

        USB_Cdc_Get_Desc_Info(cdc_obj_ptr, USB_CDC_INTERFACE_COUNT, &max_if_count);

        cdc_obj_ptr->max_supported_interfaces = max_if_count;

The first call appears to be dead.  ep_count is not used anywhere after it is set.

The second call, and the setting of max_supported_interfaces, is RNDIS-specific.  max_supported_interfaces is only used in routine PSTN_Rndis_Message_Set(), in usb_cdc_pstn.c, at lines 615-616:

    if(!(cdc_pstn_ptr->current_interface <

         cdc_obj_ptr->max_supported_interfaces))

I'd like to suggest that lines 406-407 be deleted, as dead code.

I'd further like to suggest that lines 408-410 be guarded as follows:

#if USBCFG_DEV_RNDIS_SUPPORT

        /* Get count of interfaces for a specific configuration */

        USB_Cdc_Get_Desc_Info(cdc_obj_ptr, USB_CDC_INTERFACE_COUNT, &max_if_count);

        cdc_obj_ptr->max_supported_interfaces = max_if_count;

#endif

And, while we're on the subject, in file usb_cdc.h, lines 130-134:

    uint8_t                                      max_supported_interfaces;

#if USBCFG_DEV_RNDIS_SUPPORT  

    /* rndis specific configuration */

    usb_rndis_info_struct_t                      rndis_info;

#endif

should probably be rearranged to:

#if USBCFG_DEV_RNDIS_SUPPORT

    uint8_t                                      max_supported_interfaces;

    /* rndis specific configuration */

    usb_rndis_info_struct_t                      rndis_info;

#endif

标签 (2)
2 回复数

1,988 次查看
b42754
NXP Employee
NXP Employee

Hi, John

Thanks for your comments!

(1). This is indeed a dead code. We will remove it in next release.

(2). It will be treated as RNDIS-specific in next release.

Good suggestion! Thanks again!:smileyhappy:

1,988 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi John,

I have reported this to USB stack team, and will let you know when I have any feedback.Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复