32 bit bus in multiplexed mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

32 bit bus in multiplexed mode

877 次查看
immanuelraja
Contributor I

Hi, I am using TWR-K60F120M tower , I want to configure 32 bit bus in multiplexed mode. Please suggest the Register   configuration (The board is working fine in 16 bit non multiplexed mode).

0 项奖励
回复
1 回复

824 次查看
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Immanuel,

If you use 32 bits multiplexed mode, from hardware perspective, you have to use 32 bits latch device to latch the address in the address stage of FlexBus timing.

From software perspective, you have to set the port size bits FB_CSCRn[ps]=00 in binary, and set the FB_CSPMCR register if you use byte enbale signals.

Hope it can help you

BR

Xiangjun Rong

0 项奖励
回复