10 mV anlog output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

10 mV anlog output

1,300件の閲覧回数
danielegener
Contributor I

Hi,

i am working with FRDM-K20D50M and i need an 10 mV output voltage.

How can i do this? I am not sure that this is possible with the DAC or PWM module.

Thanks in advanced!

ラベル(1)
0 件の賞賛
返信
1 返信

1,209件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi daniel

The Freedom K20 has a MK20DX128VLH5 device on LQFP64, unfortunately this device only has the 6-bit DAC key, that only can route to the internal comparator input, it does not have the option to put it to an external pin.

Others K20 like the K20_100 MHz has this option with the 12-bit Digital-to-Analog Converter (DAC), but not the K20_50 MHz.


Regarding to do it with the PWM,I believe that is not a good option,  you only can control the pulse width, but not the voltage, so you will have a signal that if you measure you can get the 10mV ( average of the DC voltage) but the true is that you will have a signal with a little time on high and long time on low, I do not know what is your application, but probably this kind of signal are not properly for your application and also this signal can get electrical noise.


Regards

Vicente Gomez

0 件の賞賛
返信