use the Debugger to examine and modify data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

use the Debugger to examine and modify data

2,763件の閲覧回数
abby
Contributor I

Hi All,

 

CodeWarrior has this function:  use the CodeWarrior Debugger to examine and modify data

http://www.freescale.com/files/training_pdf/24633_CW_DEBUGGER_DATA_WBT.pdf?lang_cd=ja

Does KDS have this function, too?

Because I can't add variables to variables windows in KDS.

Thanks.

 

Abby

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,558件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Abby,

KDS is using Eclipse Kepler, so this applies:

Variable Debugging with Eclipse Kepler | MCU on Eclipse

I hope this helps,

Erich

0 件の賞賛
返信

2,558件の閲覧回数
abby
Contributor I

Hi Erich,

Thanks for your reply.

I need to modify variables but not view data only. (when CPU is running)

In KDS, I can add global variables to the expressions but can't modify the value when CPU is running.

The global variables only can be changed value when CPU is halt in KDS.


Abby

0 件の賞賛
返信

2,558件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Abby,

modifying variables while the target is running is a CodeWarrior specific extension, and not supported in stock Eclipse Kepler/CDT as used in Kinetis Design Studio.

See http://mcuoneclipse.com/2014/09/28/comparing-codewarrior-with-kinetis-design-studio/

Erich

0 件の賞賛
返信

2,558件の閲覧回数
dporada
Contributor III

Do you think that KDS will ever support these features?  We switched to Freescale because of the advanced debugging including the ability use trace.

0 件の賞賛
返信

2,558件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Until CDT will add that functionality, I'm affraid that KDS won't support this.

0 件の賞賛
返信