use the Debugger to examine and modify data

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

use the Debugger to examine and modify data

1,786 次查看
abby
Contributor I

Hi All,

 

CodeWarrior has this function:  use the CodeWarrior Debugger to examine and modify data

http://www.freescale.com/files/training_pdf/24633_CW_DEBUGGER_DATA_WBT.pdf?lang_cd=ja

Does KDS have this function, too?

Because I can't add variables to variables windows in KDS.

Thanks.

 

Abby

标签 (1)
0 项奖励
回复
5 回复数

1,582 次查看
BlackNight
NXP Employee
NXP Employee

Hi Abby,

KDS is using Eclipse Kepler, so this applies:

Variable Debugging with Eclipse Kepler | MCU on Eclipse

I hope this helps,

Erich

0 项奖励
回复

1,582 次查看
abby
Contributor I

Hi Erich,

Thanks for your reply.

I need to modify variables but not view data only. (when CPU is running)

In KDS, I can add global variables to the expressions but can't modify the value when CPU is running.

The global variables only can be changed value when CPU is halt in KDS.


Abby

0 项奖励
回复

1,582 次查看
BlackNight
NXP Employee
NXP Employee

Hi Abby,

modifying variables while the target is running is a CodeWarrior specific extension, and not supported in stock Eclipse Kepler/CDT as used in Kinetis Design Studio.

See http://mcuoneclipse.com/2014/09/28/comparing-codewarrior-with-kinetis-design-studio/

Erich

0 项奖励
回复

1,582 次查看
dporada
Contributor III

Do you think that KDS will ever support these features?  We switched to Freescale because of the advanced debugging including the ability use trace.

0 项奖励
回复

1,582 次查看
BlackNight
NXP Employee
NXP Employee

Until CDT will add that functionality, I'm affraid that KDS won't support this.

0 项奖励
回复