software upgradation question for kl26z microcontrollers

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

software upgradation question for kl26z microcontrollers

2,552 Views
jayanthvasisht
Contributor II

Hi Everyone,

 

I read a blog on using SWD to upgrade the software on my target MCU. My goal is not use OpenSDA as it is not helpful for production releases.

Are there any other way to upgrade the target mcu without using swd. Something like DFU upgrade where in I just plugin my usb port to pc and upgrade.

Please throw some light on the same. Share some information if anyone has worked on it.

To use SWD we need a P & E multilink interface. So is that only option? Thanks in advance.Kinetis Design StudioKinetis Software Development Kit@

 

Regards

Jayanth BR

Labels (1)
0 Kudos
Reply
3 Replies

2,381 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Jayanth,

The KBOOT 1.2.0 allows the target device to upgrade the software through the UART, I2C,SPI, UART or USB HID.

As David mentioned above, the KBOOT hasn't provided the corresponding demo for KL26, however for KL25.

And I'd like to suggest that you can port this demo to KL26 through the steps that the attachment illustrates.

2015-10-19_13-39-37.jpg
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,381 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jayanth BR,

please check if this document can help you.

the bootloader works for both single and multi devices.

the demo code based on KL26

SW and video are all attached.

Kinetis Bootloader to Update Multiple Devices in a Network - for Cortex-M0+

can this help you?

Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,381 Views
DavidS
NXP Employee
NXP Employee

Hi Jayanth,

Currently the best solution is PEMicro SWD interface.

KBOOT doesn't currently support KL26Z.

Regards,

David

0 Kudos
Reply