problem writting 2d arrays into SD card

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

problem writting 2d arrays into SD card

跳至解决方案
5,341 次查看
arunkumar1989
Contributor I

Hey guys,

 

I am having some problem writing 2D arrays into SD card.

Please consider the following example:

[code]

int16 Ringbuf[5][2] = { {0,0}, {1,2}, {2,4}, {3,6},{4,8}};

 

FAT1_f_printf(&fs,"%d,",Ringbuf[0,0);     //random garbage is being written to file here.

 

[/code]

 

Any idea why this is happening?

I am using MK60MOVLQF15 CPU

 

Thanks,

Arun

标签 (1)
0 项奖励
回复
1 解答
5,237 次查看
BlackNight
NXP Employee
NXP Employee

Change

FAT1_f_printf(&fs,"%d,",Ring[0,1]);

to

FAT1_f_printf(&fs,"%hd,",Ring[0][1]);

在原帖中查看解决方案

0 项奖励
回复
8 回复数
5,237 次查看
BlackNight
NXP Employee
NXP Employee

Hi Arun,

I think I have not really used that printf() function.

printf() uses a lot of stack, make sure you have plenty stack space allocated.

Then, %d is for integer, probably 32bit on your microcontroller.

Use %hd instead (see printf - C++ Reference ).

Maybe this explains what is happening.

I hope this helps,

Erich

0 项奖励
回复
5,237 次查看
arunkumar1989
Contributor I

no luck so far ,single dimensional arrays are working correctly,my problem is with 2D arrays,the manual also has no examples with 2D examples are given,is there any way around this?

FatFs - f_printf

0 项奖励
回复
5,237 次查看
BlackNight
NXP Employee
NXP Employee

if the array is one or two (or more) dimensional, really should not matter.

Anway, what you have pasted will not compile anyway, I think you wanted to have this:

FAT1_f_printf(&fs,"%d,",Ringbuf[0][0]);     //random garbage is being written to file here.

The other thing to check: is your code warning-free?

Make sure you have included "Fat1.h" before using any function of it, especially functions with open argument lists.

Erich

0 项奖励
回复
5,236 次查看
arunkumar1989
Contributor I

The warning at that line is this:

Description    Resource    Path    Location    Type

left-hand operand of comma expression has no effect [-Wunused-value] passing argument 1 of 'f_printf' from incompatible pointer type [enabled by default]    sdcard.c    /sdcard_150_v2/Sources    line 55    C/C++ Problem

0 项奖励
回复
5,237 次查看
BlackNight
NXP Employee
NXP Employee

So is fs really of type FIL?

0 项奖励
回复
5,234 次查看
arunkumar1989
Contributor I

Yes sir it is.

I am attaching the .c file for your reference.

This is what i am getting in the file:

536805384,

0 项奖励
回复
5,238 次查看
BlackNight
NXP Employee
NXP Employee

Change

FAT1_f_printf(&fs,"%d,",Ring[0,1]);

to

FAT1_f_printf(&fs,"%hd,",Ring[0][1]);

0 项奖励
回复
5,234 次查看
arunkumar1989
Contributor I

Yes ,a silly typo from me ,thanks that did the trick.

Thanks a lot.

AK

0 项奖励
回复