printf to the Console of KDS?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

printf to the Console of KDS?

1,722 Views
_ZZ_
Contributor II

Hello everybody,

it is me again with another question, I must thanks anybody who can help with this one.

I am working on an application which runs on a Cortex M4 K20 micro. the project is pretty complex though. I am using KSDK 1.3 and MQX 4.2, KSDK variant as well.

I wonder if anybody has managed to output streams (data) to the console of the Kinetis Design Studio IDE. 

I have had a very extended research on this and people say it is possible, but nobody knows how exactly.  

basically I would like to output my printf to the console of the KDS. 

many thanks in advance,

Regards,

Roosbeh

0 Kudos
Reply
2 Replies

1,255 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Roosbeh.

I would suggest refer these two articles from Erich

https://mcuoneclipse.com/2015/04/23/semihosting-with-gnu-arm-embedded-launchpad-and-kinetis-design-s...

https://mcuoneclipse.com/2014/06/06/semihosting-with-kinetis-design-studio/

Can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,255 Views
_ZZ_
Contributor II

 I will let you know, it might take me few days to get back to it.

thank you very much 

0 Kudos
Reply