The linker is misinterpreting one of the object file names: fsl_flexbus_hal.o is seen by the linker as fsl_flebus_hal.o (see linker invocation capture below). The output name from the compiler is correct and file fsl_flexbus_hal.o exists where it is supposed to be. The input name to the linker is correct in the list of object files to link. How do I fix this error?
16:21:08 **** Incremental Build of configuration Debug for project 1034X08_Configuration_Module_BLT ****
make all
'Building file: ../SDK/platform/hal/src/flexbus/fsl_flexbus_hal.c'
'Invoking: Cross ARM C Compiler'
arm-none-eabi-gcc -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -Wall -g3
..
..
..
MT"SDK/platform/hal/src/flexbus/fsl_flexbus_hal.o" -c -o "SDK/platform/hal/src/flexbus/fsl_flexbus_hal.o" "../SDK/platform/hal/src/flexbus/fsl_flexbus_hal.c"
'Finished building: ../SDK/platform/hal/src/flexbus/fsl_flexbus_hal.c'
' '
'Building target: 1034X08_Configuration_Module_BLT.elf'
'Invoking: Cross ARM C++ Linker'
arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -Wall -g3
..
..
..
./SDK/platform/hal/src/flexbus/fsl_flexbus_hal.o
..
..
arm-none-eabi-g++: error: ./SDK/platform/hal/src/flexbus/fsl_flebus_hal.o: No such file or directory
make: *** [1034X08_Configuration_Module_BLT.elf] Error 1
16:21:11 Build Finished (took 3s.496ms)
已解决! 转到解答。
Hi Randy,
there is a known problem on Windows with a 8192 command line character limit. One symptom is that it cuts out some characters. See Solving the 8192 Character Command Line Limit on Windows | MCU on Eclipse for the description and the solution.
I hope this helps,
Erich
Hi Randy,
there is a known problem on Windows with a 8192 command line character limit. One symptom is that it cuts out some characters. See Solving the 8192 Character Command Line Limit on Windows | MCU on Eclipse for the description and the solution.
I hope this helps,
Erich