make: *** [Static_Code/System/PE_low_level_init.o] Error 1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

make: *** [Static_Code/System/PE_low_level_init.o] Error 1

2,812 Views
nícolasludwig
Contributor II

Hi everyone.

I'm having a problem when compiling a little and simple project (just to blink a led in the FRDM-KL27Z plataform). When I do it, I get this message that you can see on the image below.

error 1.png

I just don't know what to do, I've tried everything, but the error persist. I also tried the same code in another computer, and it worked perfectly, and I did the same thing as in my computer.

I'm using:

Kinetis Design Studio 3.0.0 IDE;

Plataform: FRDM-KL27Z;

Kinetis SDK 1.3.0;

Windows 10 (I had the same error in Windows 8).

 

Can you help me?

Thanks in advance.

0 Kudos
Reply
4 Replies

2,623 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

Please upload your KDS demo code, thus we can check it directly on my side.

Thanks.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,623 Views
nícolasludwig
Contributor II

Code below:

 

/* ###################################################################
** Filename : main.c
** Project : testando
** Processor : MKL27Z64VLH4
** Version : Driver 01.01
** Compiler : GNU C Compiler
** Date/Time : 2018-03-11, 16:06, # CodeGen: 0
** Abstract :
** Main module.
** This module contains user's application code.
** Settings :
** Contents :
** No public methods
**
** ###################################################################*/
/*!
** @file main.c
** @version 01.01
** @brief
** Main module.
** This module contains user's application code.
*/ 
/*!
** @addtogroup main_module main module documentation
** @{
*/ 
/* MODULE main */


/* Including needed modules to compile this module/procedure */
#include "Cpu.h"
#include "Events.h"
#include "clockMan1.h"
#include "pin_init.h"
#include "osa1.h"
#include "gpio1.h"
#if CPU_INIT_CONFIG
#include "Init_Config.h"
#endif
/* User includes (#include below this line is not maintained by Processor Expert) */

/*lint -save -e970 Disable MISRA rule (6.3) checking. */
int main(void)
/*lint -restore Enable MISRA rule (6.3) checking. */
{
/* Write your local variable definition here */

/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
PE_low_level_init();
/*** End of Processor Expert internal initialization. ***/
int delay = 2000000;
/* Write your code here */
for(;;) {
GPIO_DRV_TogglePinOutput(LEDRGB_GREEN);
while(delay--);
delay = 2000000;

}

/*** Don't write any code pass this line, or it will be deleted during code generation. ***/
/*** RTOS startup code. Macro PEX_RTOS_START is defined by the RTOS component. DON'T MODIFY THIS CODE!!! ***/
#ifdef PEX_RTOS_START
PEX_RTOS_START(); /* Startup of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of RTOS startup code. ***/
/*** Processor Expert end of main routine. DON'T MODIFY THIS CODE!!! ***/
for(;;){}
/*** Processor Expert end of main routine. DON'T WRITE CODE BELOW!!! ***/
} /*** End of main routine. DO NOT MODIFY THIS TEXT!!! ***/

/* END main */
/*!
** @}
*/
/*
** ###################################################################
**
** This file was created by Processor Expert 10.5 [05.21]
** for the Freescale Kinetis series of microcontrollers.
**
** ###################################################################
*/

0 Kudos
Reply

2,623 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Could you please upload your entire project instead piece of code? Thanks.

Jennie Zhang

0 Kudos
Reply

2,623 Views
nícolasludwig
Contributor II

Hello.

If it helps, I posted my entire project on Google Drive, it's a .rar file. Link below:

testando.rar - Google Drive 

Thanks for your support.

0 Kudos
Reply