linker errors "multiple defintion of" when migrating from KDS 2.0 to 3.1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

linker errors "multiple defintion of" when migrating from KDS 2.0 to 3.1

跳至解决方案
3,913 次查看
mike1974
Contributor III

I had a project that built fine on KDS 2.0, but now that I have upgraded to KDS 3.1 I get the linker errors below.  I followed the migrating procedure (using the KDS Upgrade Assistant) as described here: Kinetis Design Studio: Migrating KDS V2.0.0 Projects to GNU Tools for ARM Embedded (Launchpad, KDS V... 

 

I am building a Segger graphics library first (emWin_V528b), then linking to that library in my application (called A9950V0002).  Any help would be appreciated.

 

-Mike

 

**************************

 

'Building target: A9950V0002_dbg.elf'

'Invoking: Cross ARM C++ Linker'

arm-none-eabi-g++ -mcpu=cortex-m4 -mthumb -mfloat-abi=hard -mfpu=fpv4-sp-d16 -O0 -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections  -g3 -T "C:/Users/Mike/workspace.kds/A9950V0002/Project_Settings/Linker_Files/ProcessorExpert.ld" -Xlinker --gc-sections -L"C:/Users/Mike/workspace.kds/A9950V0002/Project_Settings/Linker_Files" -L"C:\Users\Mike\workspace.kds\emWin_V528b\Debug" -Wl,-Map,"A9950V0002_dbg.map" --specs=nano.specs -o "A9950V0002_dbg.elf" @ObjectList

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `_cleanup_r':

findfp.c:(.text._cleanup_r+0x0): multiple definition of `_cleanup_r'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text._cleanup_r+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__sfmoreglue':

findfp.c:(.text.__sfmoreglue+0x0): multiple definition of `__sfmoreglue'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__sfmoreglue+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `_cleanup':

findfp.c:(.text._cleanup+0x0): multiple definition of `_cleanup'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text._cleanup+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__sinit':

findfp.c:(.text.__sinit+0x0): multiple definition of `__sinit'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__sinit+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__sfp':

findfp.c:(.text.__sfp+0x0): multiple definition of `__sfp'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__sfp+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__sfp_lock_acquire':

findfp.c:(.text.__sfp_lock_acquire+0x0): multiple definition of `__sfp_lock_acquire'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__sfp_lock_acquire+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__sfp_lock_release':

findfp.c:(.text.__sfp_lock_release+0x0): multiple definition of `__sfp_lock_release'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__sfp_lock_release+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__sinit_lock_acquire':

findfp.c:(.text.__sinit_lock_acquire+0x0): multiple definition of `__sinit_lock_acquire'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__sinit_lock_acquire+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__sinit_lock_release':

findfp.c:(.text.__sinit_lock_release+0x0): multiple definition of `__sinit_lock_release'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__sinit_lock_release+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__fp_lock_all':

findfp.c:(.text.__fp_lock_all+0x0): multiple definition of `__fp_lock_all'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__fp_lock_all+0x0): first defined here

c:/freescale/kds_3.0.0/toolchain/bin/../lib/gcc/arm-none-eabi/4.8.4/../../../../arm-none-eabi/lib/armv7e-m/fpu\libg_s.a(lib_a-findfp.o): In function `__fp_unlock_all':

findfp.c:(.text.__fp_unlock_all+0x0): multiple definition of `__fp_unlock_all'

C:/Freescale/KDS_2.0.0/toolchain/arm-none-eabi/lib/m4/fp/v4-sp-d16/libc.a(lib_a-findfp.o):(.text.__fp_unlock_all+0x0): first defined here

collect2.exe: error: ld returned 1 exit status

make: *** [A9950V0002_dbg.elf] Error 1

标签 (1)
1 解答
2,989 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

the errors show us that the same symbol is included in two files.

for example, symbol "_cleanup_r"  is detected in both of these two files which are both included in your project:

pastedImage_0.png

to solve the problem:

- Please go to your project properties setting, remove all KDS2.0 related path and included files.

- go to IDE menu "project", "clean" to clean the old file associations.

can this help you? if not, please post your project here, we can help you check the problem directly.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

3 回复数
2,990 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

the errors show us that the same symbol is included in two files.

for example, symbol "_cleanup_r"  is detected in both of these two files which are both included in your project:

pastedImage_0.png

to solve the problem:

- Please go to your project properties setting, remove all KDS2.0 related path and included files.

- go to IDE menu "project", "clean" to clean the old file associations.

can this help you? if not, please post your project here, we can help you check the problem directly.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,989 次查看
mike1974
Contributor III

Thanks Jennie, I found out the references to KDS_2.0.0 were in a file "makefile.defs".  This file was used to correct a problem in KDS_2.0.0 described here:

KSDK Linker Error - Command line too long

Does KDS 3.1 still have that problem? 

0 项奖励
回复
2,989 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Michael,

you are welcome.

according to KDS3.1 release note, this "Windows Command Line Limit" issue is still a known issue which is not fixed yet.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复