kinetis design studio headless java error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kinetis design studio headless java error

1,928件の閲覧回数
netstv73
Contributor III

KDS Details:

Kinetis Design Studio

Version: 3.2.0

©Freescale Semiconductor, Inc. 2016. All rights reserved.

Kinetis Design Studio includes features from GNU ARM Eclipse plug-ins http://gnuarmeclipse.livius.net

and from SOMNIUM® Technologies http://www.somniumtech.com

Eclipse Version: Luna SR2 (4.4.2)

SOMNIUM® is a registered trademark of SOMNIUM® Technologies Limited. Freescale and Kinetis are trademarks of Freescale Semiconductor, Inc., Reg. U.S. Pat. & Tm. Off.

OSX Sierra

ksdk 1.2.0 (because we use mqx and need to stick to this version).

I have issues running the following command:

/Applications/KDS_v3.app//Contents/eclipse/kinetis-design-studio -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild -importAll /Users/steveiribarne/work/my_proj/external

and I get the error as a GIANT Alert Dialog box....

Java was started but returned exit code=1

-Dosgi.requiredJavaVersion=1.7

-Xms256m

-Xmx512m

-XX:PermSize=256m

-XX:MaxPermSize=512m

-XstartOnFirstThread

-Dorg.eclipse.swt.internal.carbon.smallFonts

-Djava.class.path=/Applications/KDS_v3.app/Contents/eclipse//plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar

-os macosx

-ws cocoa

-arch x86_64

-launcher /Applications/KDS_v3.app/Contents/eclipse/kinetis-design-studio

-name Kinetis Design Studio

--launcher.library /Applications/KDS_v3.app/Contents/eclipse//plugins/org.eclipse.equinox.launcher.cocoa.macosx.x86_64_1.1.200.v20150204-1316/eclipse_1607.so

-startup /Applications/KDS_v3.app/Contents/eclipse//plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar

--launcher.overrideVmargs

-product com.somniumtech.branding.kds.ide

-application org.eclipse.cdt.managedbuilder.core.headlessbuild

-importAll /Users/steveiribarne/work/my_proj/external

-vm /Applications/KDS_v3.app/Contents/eclipse/features/com.somniumtech.jre.macosx.cocoa.x86_64_1.7.0.76/jre/Contents/Home/lib/jli/libjli.dylib

-vmargs

-Dosgi.requiredJavaVersion=1.7

-Xms256m

-Xmx512m

-XX:PermSize=256m

-XX:MaxPermSize=512m

-XstartOnFirstThread

-Dorg.eclipse.swt.internal.carbon.smallFonts

-Djava.class.path=/Applications/KDS_v3.app/Contents/eclipse//plugins/org.eclipse.equinox.launcher_1.3.0.v20140415-2008.jar

I have Java version 1.8.  I've tried 1.7 but I get the same error.

In my_proj/external are the ksdk library projects.  On the command line I get 

Project: ksdk_mqx_lib already exists in the workspace!

I don't know the first thing about how to debug this...

Can you shed some light on this for me please?

Thank you.

-steve

0 件の賞賛
返信
2 返答(返信)

1,645件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Steve,

your problem is that you try to import a project into the workspace, but that project already exists in that workspace. You cannot have two projects with the same name in the workspace.

Articles which describe the command line options building with Eclipse:

Building Projects with Eclipse from the Command Line | MCU on Eclipse 

Building Eclipse and MCUXpresso IDE Projects from the Command Line | MCU on Eclipse 

I hope this helps,

Erich

0 件の賞賛
返信

1,645件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Steve,

about GIANT dialog - this is a way, how Java reports that the application returned non zero exit code.

About debugging, I'd suggest to try the same operation in KDS UI.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信