how do i connect freedom to arduino

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

how do i connect freedom to arduino

跳至解决方案
1,460 次查看
roberthalversen
Contributor I

I have a Freedom FRDM-KE022Z40M which is not supplied with connectors.  I found 0.100" female headers from Digikey that should fit but I do not understand how this will mate with Arduino R3 boards.  Does Freescale (NXP) have recommended connectors that will allow me to connect to the Arduino board?  Do you have any pictures showing the two boards connected?

 

Robert

标签 (1)
0 项奖励
回复
1 解答
1,275 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Robert,

I don't have experience on connecting FRDM with Arduino R3 board. But I know Erich ever wrote a set of articles on this related. Can you please check if this can be helpful to you:

https://mcuoneclipse.com/2012/09/28/kl25z-freedom-board-and-arduino-headers/

https://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/

https://mcuoneclipse.com/2014/01/05/frdm-with-ardino-ethernet-shield-r3-part-1-sd-card/


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
1,276 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Robert,

I don't have experience on connecting FRDM with Arduino R3 board. But I know Erich ever wrote a set of articles on this related. Can you please check if this can be helpful to you:

https://mcuoneclipse.com/2012/09/28/kl25z-freedom-board-and-arduino-headers/

https://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/

https://mcuoneclipse.com/2014/01/05/frdm-with-ardino-ethernet-shield-r3-part-1-sd-card/


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------