how do i connect freedom to arduino

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how do i connect freedom to arduino

Jump to solution
1,478 Views
roberthalversen
Contributor I

I have a Freedom FRDM-KE022Z40M which is not supplied with connectors.  I found 0.100" female headers from Digikey that should fit but I do not understand how this will mate with Arduino R3 boards.  Does Freescale (NXP) have recommended connectors that will allow me to connect to the Arduino board?  Do you have any pictures showing the two boards connected?

 

Robert

Labels (1)
0 Kudos
Reply
1 Solution
1,293 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Robert,

I don't have experience on connecting FRDM with Arduino R3 board. But I know Erich ever wrote a set of articles on this related. Can you please check if this can be helpful to you:

https://mcuoneclipse.com/2012/09/28/kl25z-freedom-board-and-arduino-headers/

https://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/

https://mcuoneclipse.com/2014/01/05/frdm-with-ardino-ethernet-shield-r3-part-1-sd-card/


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
1,294 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Robert,

I don't have experience on connecting FRDM with Arduino R3 board. But I know Erich ever wrote a set of articles on this related. Can you please check if this can be helpful to you:

https://mcuoneclipse.com/2012/09/28/kl25z-freedom-board-and-arduino-headers/

https://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/

https://mcuoneclipse.com/2014/01/05/frdm-with-ardino-ethernet-shield-r3-part-1-sd-card/


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------