how do i connect freedom to arduino

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

how do i connect freedom to arduino

ソリューションへジャンプ
1,473件の閲覧回数
roberthalversen
Contributor I

I have a Freedom FRDM-KE022Z40M which is not supplied with connectors.  I found 0.100" female headers from Digikey that should fit but I do not understand how this will mate with Arduino R3 boards.  Does Freescale (NXP) have recommended connectors that will allow me to connect to the Arduino board?  Do you have any pictures showing the two boards connected?

 

Robert

ラベル(1)
0 件の賞賛
返信
1 解決策
1,288件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Robert,

I don't have experience on connecting FRDM with Arduino R3 board. But I know Erich ever wrote a set of articles on this related. Can you please check if this can be helpful to you:

https://mcuoneclipse.com/2012/09/28/kl25z-freedom-board-and-arduino-headers/

https://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/

https://mcuoneclipse.com/2014/01/05/frdm-with-ardino-ethernet-shield-r3-part-1-sd-card/


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,289件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello Robert,

I don't have experience on connecting FRDM with Arduino R3 board. But I know Erich ever wrote a set of articles on this related. Can you please check if this can be helpful to you:

https://mcuoneclipse.com/2012/09/28/kl25z-freedom-board-and-arduino-headers/

https://mcuoneclipse.com/2012/12/14/frdm-kl25z-with-the-arduino-motor-shield/

https://mcuoneclipse.com/2014/01/05/frdm-with-ardino-ethernet-shield-r3-part-1-sd-card/


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------