d

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
1,322 Views
dungwang
Contributor I

e

0 Kudos
Reply
1 Solution
1,163 Views
BlackNight
NXP Employee
NXP Employee

Hello Dung,

the reason is that on Kinetis K there are two memory controllers, one for each memory area. Because it can cause a hard fault if you are accessing the memory boundary with an unaligned access, the two memory areas are splitted. If you ensure that you do not have any misaligned access, you can combine the two areas. See the comments section of FreeRTOS Heap with Segmented Kinetis K SRAM | MCU on Eclipse  for a detailed discusson on that topic.

I hpe this helps,

Erich

View solution in original post

1 Reply
1,164 Views
BlackNight
NXP Employee
NXP Employee

Hello Dung,

the reason is that on Kinetis K there are two memory controllers, one for each memory area. Because it can cause a hard fault if you are accessing the memory boundary with an unaligned access, the two memory areas are splitted. If you ensure that you do not have any misaligned access, you can combine the two areas. See the comments section of FreeRTOS Heap with Segmented Kinetis K SRAM | MCU on Eclipse  for a detailed discusson on that topic.

I hpe this helps,

Erich