bug report : can not add dspi component in linux, for missing fsl_dspi_edma component.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

bug report : can not add dspi component in linux, for missing fsl_dspi_edma component.

1,106 Views
rqbh
Contributor III

when add a dspi component into project, there is a error shows can not add fsl_dspi_edma component in linux . but in windows, there is no that error.

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

956 Views
rqbh
Contributor III

Is no anyone else meet that problem ?

0 Kudos
Reply

956 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Kevin,

Do you installed the version  "KSDK_1.0.0_INSTALL_LINUX"  ?

Alice

0 Kudos
Reply

956 Views
rqbh
Contributor III

yes ,i have installed, the other components are worked ok, only dspi component show that error message.

0 Kudos
Reply