about MK22FN512's External bus clock

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

about MK22FN512's External bus clock

1,266 次查看
andypeng
Contributor I

Hi,

   I use KSDK1.3.0 component library version set MK22FN512 clock system in KDS, found the external bus clock maximum is 30MHz, but if the kinetis component library version external bus clock maximum is 60MHz. this is what reason? I would like to work in KSDK1.3.0 component library version so that the external bus clock works at 60MHz, can you?

173866_173866.pngpastedImage_3.png

173865_173865.pngpastedImage_2.png

 

 

Thank you

Andy

标签 (1)
0 项奖励
回复
1 回复

1,116 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andy,

Please check the Reference Manual of MK22FN512VLL12,

the Maximum FlexBus clock(External bus clock) is 30MHZ.

pastedImage_1.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复