Will KDS handle .s ARM assembly code?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will KDS handle .s ARM assembly code?

ソリューションへジャンプ
1,696件の閲覧回数
nirvanauscn
Contributor III

KDS only handles .asm and .S as valid assembly code files, and the preference is locked and can't be modified or added

(Preference -> General -> Content Types -> Text -> Assembly Source File).

 

For the projects I'm working on, all assembly files are in .s postfix instead of .S, and KDS just simply ignore them.

Is there a way to add .s support?

 

Is this a feature or defect?

 

Only Linux is in real case-sensitive file system, both Windows and OS X (can be case sensitive, but the home drive normally isn't setup that way) are case aware, but not case sensitive.

 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,416件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I've found the following:

    Bug 105022 – [content type] file specs should be case-sensitive

    Bug 103530 – managed build: File with capital "S" extension not recognized as assembly

Adding a new File types for .s is not working due to the case sensitive problem.

Now the workaround is to add .s types in the project properties.

    Bug 278026 – Managed build doesn't work for *.s assembler files

Extract:

+++++++++++++++++++++++++++

In the meantime I found a workaround for the problem:

Project Properties -> C/C++ General -> File Types -> Use project settings -> New -> Pattern: *.s, Type: Assembly Source File -> OK

+++++++++++++++++++++++++++

I've checked it on my side and it's working.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,416件の閲覧回数
nirvanauscn
Contributor III

Thanks, adding .s to the project setting addressed the issue.

0 件の賞賛
返信
1,417件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi,

I've found the following:

    Bug 105022 – [content type] file specs should be case-sensitive

    Bug 103530 – managed build: File with capital "S" extension not recognized as assembly

Adding a new File types for .s is not working due to the case sensitive problem.

Now the workaround is to add .s types in the project properties.

    Bug 278026 – Managed build doesn't work for *.s assembler files

Extract:

+++++++++++++++++++++++++++

In the meantime I found a workaround for the problem:

Project Properties -> C/C++ General -> File Types -> Use project settings -> New -> Pattern: *.s, Type: Assembly Source File -> OK

+++++++++++++++++++++++++++

I've checked it on my side and it's working.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信