When will the MKV56F512VLL20 will be supported by Processor Expert?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

When will the MKV56F512VLL20 will be supported by Processor Expert?

1,739件の閲覧回数
erskineb
Contributor I

Can I get a date when MKV56F512VLL20 will be supported by Processor Expert?

And until that time can you give a PN for a Core M7 part that is supported by Processor Expert so I can get a head start?

If neither of the above is possible anytime soon can you give me a part similar to the MKV56F512VLL20 that will port to MKV56F512VLL20?

I was given MKV31F51212 in a past question as a similar part, but there is nothing I can find that states the work I do on this part is transferable to the MKV56F512VLL20.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,574件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

Per feedback from processor expert team,

processor expert for MKV56 and MKV58 derivatives will be included in SDK 1.3. GA (final) version. and should be deployed to public KEx server in upcoming days.

Just a notice regarding MKV56F512VLL20. It is 200MHz part, which was discontinued. Going forward, only 240MHz parts will be offered to customers (MKV56F512xxx24).


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,574件の閲覧回数
erskineb
Contributor I

Hi,

Thanks for your response.We will plan accordingly.

Best Regards,Erskine Barbour

From: ZhangJennie <[email protected]>

To: Erskine Barbour <[email protected]>

Sent: Wednesday, May 11, 2016 11:15 PM

Subject: Re: - When will the MKV56F512VLL20 will be supported by Processor Expert?

#yiv8788467991 * #yiv8788467991 a #yiv8788467991 body {font-family:Helvetica, Arial, sans-serif;}#yiv8788467991 #yiv8788467991 h1, #yiv8788467991 h2, #yiv8788467991 h3, #yiv8788467991 h4, #yiv8788467991 h5, #yiv8788467991 h6, #yiv8788467991 p, #yiv8788467991 hr {}#yiv8788467991 .yiv8788467991button td {}

|

NXP Community

|

When will the MKV56F512VLL20 will be supported by Processor Expert?

reply from ZhangJennie in Kinetis Microcontrollers - View the full discussionHi, Per feedback from processor expert team,processor expert for MKV56 and MKV58 derivatives will be included in SDK 1.3. GA (final) version. and should be deployed to public KEx server in upcoming days.Just a notice regarding MKV56F512VLL20. It is 200MHz part, which was discontinued. Going forward, only 240MHz parts will be offered to customers (MKV56F512xxx24).  

Have a great day,

Jennie Zhang 

0 件の賞賛
返信

1,574件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信