When I install update eclipse from help/install software, an error encounter as shown followed:

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

When I install update eclipse from help/install software, an error encounter as shown followed:

1,910 Views
林偉川
Contributor I

When I install update eclipse from help/install software, an error encounter as shown followed:

An error occurred while collecting items to be installed

session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).

Unable to read repository at http://freescale.com/lgfiles/updates/Eclipse/KDS/binary/com.freescale.processorexpert.ksdk-1.2.0.sp_....

Unexpected end of ZLIB input stream

 

Would you tell me what's wrong with it?

My PC is CPU i7 , OS is Windows 7. However, my NB is windows 8, it is OK for updating. Why??

Labels (1)
0 Kudos
Reply
1 Reply

1,617 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Lin,

Please tell which software you update , i will test it on my side , does it KSDK ?

And what about the version of KDS . I recommend you use the latest one KDS 3.0 , and install the latest KSDK 1.3 .

KDS3.0: Kinetis Design Studio Integrated Development |Freescale

KSDK1.3: https://freescale.flexnetoperations.com/control/frse/product?entitlementId=123594587&lineNum=1&authC...

If use the latest one it still have error ,please send me a screenshot about it .

Hope it helps



-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

Have a great day,
Alice

0 Kudos
Reply