What is the proper way to open an existing project?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the proper way to open an existing project?

2,261 Views
Kratz
Contributor IV

I have three different projects that I am working in KDS. Everything works fine to make a new project and work on it. However, when changing from one existing project to another, I close KDS, Open it to the workspace of the project I want to use, and then the "Open Project" is not in black so the project can be opened. What is the proper way to open an existing project?

 

~Kevin

Labels (1)
0 Kudos
Reply
2 Replies

2,048 Views
BlackNight
NXP Employee
NXP Employee

It sounds like you are using one project per workspace. But you can have multiple projects in a workspace.

Import existing projects using the menu

File > Import > General > Existing projects into workspace.

The menu Project > Open Project and Close projects are about to close and open projects which are already in the workspace.

This because in Eclipse you should not have too many projects open for performance reasons, see Eclipse Performance Improvement Tip: Close Unused Projects | MCU on Eclipse.

I hope this helps,

Erich

0 Kudos
Reply

2,048 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Kevin,

What do you mean of "the "Open Project" is not in black so the project can be opened. " ?

And , you can " click the File button ->  Switch workspace" ,  open the workspace which your project in .

Hope it helps

Alice

0 Kudos
Reply