What is more preferable IDE?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What is more preferable IDE?

3,171 次查看
alexandergoldin
Contributor III

What is more preferable IDE CodeWarrior or Kinetis?

标签 (1)
0 项奖励
回复
5 回复数

2,979 次查看
trytohelp
NXP Employee
NXP Employee

Hi Alexander,

You will find more info on the blog: MCU on Eclipse | Everything on Eclipse, Microcontrollers and Software

Refer to:

    http://mcuoneclipse.com/2014/09/28/comparing-codewarrior-with-kinetis-design-studio/

    Using Kinetis Design Studio with IAR Embedded Workbench IDE | MCU on Eclipse

     ....


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,979 次查看
alexandergoldin
Contributor III

Thank you, Pascal. I will check it.

2,979 次查看
bcamp
Contributor III

Hi

As time goes on, I don't believe that CodeWarrior for ARM will receive the attention that KDS gets. Porting between the various tools is not as simple as you might think. If you are not running anything now I would pick KDS over CW.

The more involved question is IAR vs Keil vs KDS (and others). There you are comparing "paid" options to "free" ones. The

CW / KDS decision is also paid vs free at some level.

Bob

2,979 次查看
alexandergoldin
Contributor III

Thank you, Bob. It is an interesting point of view.

2,979 次查看
alexandergoldin
Contributor III

There is an opinion, that "Usage of Kinetis Design Studio is recommended for new projects".