Using KDS on Linux Debian

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using KDS on Linux Debian

951件の閲覧回数
ludovictancerel
Contributor I

Hello,

 

I am having trouble using KDS on a Linux machine (Debian distribution).

I am a bit puzzled with this experience, I am quite experienced with Eclipse as I use it in my job.

I want to use KDS for personnal usage, but I also use it as an evaluation for my job, and well, I am not impressed.

The initial feedback is very negative as I have lost already plenty of time trying to setup the environment.

 

My board is a FRDM-KL46Z

 

The KDS deb package is installed, I am able to launch studio.

I downloaded

Installer: Kinetis Design Studio installer for Linux 64-bit DEB 3.0.0

 

After troubles in finding the appropriate tuto, I eventually was able to find how to setup Kinetis in order to be able to setup a board archive where I was able to load one of the project.

Of course it did not compile immediately...

I had to install arm-none-eabi-gcc myself. It is not explained you have to do it...

I solved the problems of missing libraries as well.

 

So now I have a compiled and linked image... Wow, This was the 3rd evening spent on this. I am not at the 5th ...

 

I am now trying to run debug configuration.

The 4th evening was spent trying using openOCD on CMSIS-DAP but I realized that the bootloader did not enumerate such interface although this is what is documented.

I downloaded an more recent bootloader which still does not enumerate CMSIS-DAP and figured out I should be using openSDA, although I am not sure.

 

After reading "Writing my first KSDK Application in KDS - Appendix C"

as well as reading http://www.nxp.com/files/32bit/doc/user_guide/OPENSDAUG.pdf (well I don't read all, I just want to do an evaluation)

I downloaded & ran a setup from P&E website, which apparently setups the udev rules even if it is not explicitly said. This still does not solve my problem

 

I wonder whether I am missing anything, anyway,

I am tired to try and unless anyone providesd me clear explanations on what's going-on I will buy an evaluation board from a different company.

 

I would like to provide a better status but this is so messy that I don't remember all the links I have been to, and what exactly I did at the end.

 

Below is the enumeration I get in the console with dmesg.

I am able to get the

 

[ 2914.710235] usb 2-1.1: new full-speed USB device number 9 using ehci-pci

[ 2914.804649] usb 2-1.1: New USB device found, idVendor=1357, idProduct=0707

[ 2914.804655] usb 2-1.1: New USB device strings: Mfr=1, Product=2, SerialNumber=0

[ 2914.804657] usb 2-1.1: Product: PEMicro/Freescale - CDC Serial Port

[ 2914.804659] usb 2-1.1: Manufacturer: P&E Microcomputer Systems Inc.

[ 2914.805243] cdc_acm 2-1.1:1.0: This device cannot do calls on its own. It is not a modem.

[ 2914.805264] cdc_acm 2-1.1:1.0: ttyACM0: USB ACM device

[ 2914.805708] usb-storage 2-1.1:1.2: USB Mass Storage device detected

[ 2914.806666] scsi11 : usb-storage 2-1.1:1.2

[ 2915.806283] scsi 11:0:0:0: Direct-Access     FSL      FSL/PEMICRO MSD  0001 PQ: 0 ANSI: 4

[ 2915.806644] sd 11:0:0:0: Attached scsi generic sg2 type 0

[ 2915.807402] sd 11:0:0:0: [sdb] 1983999 512-byte logical blocks: (1.01 GB/968 MiB)

[ 2915.808489] sd 11:0:0:0: [sdb] Write Protect is off

[ 2915.808492] sd 11:0:0:0: [sdb] Mode Sense: 00 00 00 00

[ 2915.809109] sd 11:0:0:0: [sdb] Asking for cache data failed

[ 2915.809114] sd 11:0:0:0: [sdb] Assuming drive cache: write through

[ 2915.824244]  sdb:

[ 2915.827334] sd 11:0:0:0: [sdb] Attached SCSI removable disk

[ 2917.445005] FAT-fs (sdb): utf8 is not a recommended IO charset for FAT filesystems, filesystem will be case sensitive!

ラベル(1)
0 件の賞賛
返信
0 返答(返信)