TimerInt_LDD component

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TimerInt_LDD component

ソリューションへジャンプ
1,776件の閲覧回数
shauldorf
Contributor V

I want to implement variable period Internal Interrupt.

I’m using FRDM-K64F and KDS3.0 + KSDK1.2

Is there any solution how to change dynamically  (during runtime)  Period/Frequency of TimerInt_LDD component.

I have seen that the relevant Kinetis methods in TimerInt_LDD are not implemented.

Shaul

ラベル(1)
0 件の賞賛
返信
1 解決策
1,554件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi shaul.

TimerInt_LDD can not change frequency during runtime. I suggest you use PPG component instead, which can change output radio and frequency dynamically.

please refer this link:

Re: How to change PWM frequency

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,555件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi shaul.

TimerInt_LDD can not change frequency during runtime. I suggest you use PPG component instead, which can change output radio and frequency dynamically.

please refer this link:

Re: How to change PWM frequency

can this help you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信