The project does not appear in the Debug configurations

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The project does not appear in the Debug configurations

4,982 次查看
pietrodicastri
Senior Contributor II

Good morning

 

I have a strange problem with the KDS 3.2.0

I produced a project. It  builds correctly but it is not possible to debug, since it does not appear in the list in the Debug configurations. It is visible in the attached files.

 

If there is a good advice it could be easy to fix 

 

 

Thank You

标签 (1)
标记 (1)
8 回复数

4,824 次查看
pietrodicastri
Senior Contributor II

Ok ..

I have recreated the project from the scrap. It is now running. 

Definitely I think I put the KDS in unusual situation .. Who knows..

Thank You

0 项奖励
回复

4,824 次查看
pietrodicastri
Senior Contributor II

Thank you for the help..

I try whatever but I don t get it to work.. Something I did has now put in an inconsistent state. I will try to recreate the project.

0 项奖励
回复

4,824 次查看
BlackNight
NXP Employee
NXP Employee

Are .launch files present in your project?

0 项奖励
回复

4,824 次查看
pietrodicastri
Senior Contributor II

Hi Erich

The project Encoder003 does not appear in the list. It is an executable, actually identical to the Encoder002. For a reason I don t understand it is not possible to debug.. 

Thank You

0 项奖励
回复

4,824 次查看
pietrodicastri
Senior Contributor II

Effectively at a closer look also the Encoder002 project is not in the list. I used some time ago for debugging without any problem. Maybe the migration from a KDS  older version has created a problem???

Thank You

0 项奖励
回复

4,824 次查看
BlackNight
NXP Employee
NXP Employee

check your filters (see my answer above).

And check if the Encoder projects have .launch files in it.

Erich

0 项奖励
回复

4,824 次查看
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

that dialig lists all the .launch files inside your projects, if they reference a project, plus the ones stored in the 'framework' (if not shared as file, see Sharing Debug Configuration with Eclipse | MCU on Eclipse ). Then they are filtered too. So could it be that you have it filtered, so can you check your filters?

pastedImage_377.png

I hope this helps,

Erich

4,824 次查看
BlackNight
NXP Employee
NXP Employee

Hi Pietro,

which project?

If it is it the lib (library) project: you won't be able to debug a library project directly: you debug the project which is using the library.

I hope this helps,

Erich

0 项奖励
回复