The board FRDM K64F use. Kinetis Design Studio IDE is being programmed. I receive a compile error when using the FXOS8700CQ in the component. Is there a workaround for this part?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The board FRDM K64F use. Kinetis Design Studio IDE is being programmed. I receive a compile error when using the FXOS8700CQ in the component. Is there a workaround for this part?

1,000件の閲覧回数
youngsupark
Contributor I

The board FRDM K64F use.

Kinetis Design Studio IDE is being programmed.

I receive a compile error when using the FXOS8700CQ in the component.

Is there a workaround for this part?

 

25966_25966.JPG오류.JPG

ラベル(1)
0 件の賞賛
返信
1 返信

894件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

are all the properties of the component configured? For example like this:

pastedImage_0.png

Erich

0 件の賞賛
返信