TWR-KV58F220M debug problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-KV58F220M debug problem

1,745 Views
1029470549
Contributor I

Hi,when i am using TWR-KV58F220M, I failed to debug it via KDS and KEIL.

 

they both have error.

 

the KEIL has error like :

106203_106203.png5(HV}`_I66}N}3}A`}V(8KJ.png106205_106205.pngYX6BGWQE9~IAD)6[3I`YPQV.png

 

 

the KDS has error like:

106204_106204.png4L`6BH08@D}BLDUB@`L[2$P.png

 

I tried some solutions, the error  from KDS became

 

Error: couldn't bind to socket: No error

 

and i still can't debug it.

 

when i want to use jlink to erase the chip, I failed agin here is the error dispayed

 

D%555YNEPP1W]8W3JB]%8[6.png

 

 

 

 

How can I solve this?  THX!

Labels (1)
0 Kudos
Reply
2 Replies

1,589 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ningmeng,

- What about your project ? Could you please create one simple project , then try again ?

- And have you drag and drop the file of "JLink_OpenSDA_V2_1_2015-04-23.bin" into board

when it in the bootloader mode ? About the detail information please refer to :

TWR-KV58F220M-QSP\TWR-KV58F220M_Quick Start Package\OpenSDA Application\Segger OpenSDA

Hope it helps

Alice

0 Kudos
Reply

1,589 Views
1029470549
Contributor I

HI,I ‘ve drag and drop the file of "JLink_OpenSDA_V2_1_2015-04-23.bin" into board.

Then,i create a blank project of "MKV58F220M" processor.

but when i use Debug_Seager. It still don't work.

Below is the information KDS gived.

8P}2U5`3SF88NHCN]4LV%TH.png

0 Kudos
Reply