TWR-K64F120M and Segger J-Link Probe

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

TWR-K64F120M and Segger J-Link Probe

ソリューションへジャンプ
2,246件の閲覧回数
intractablesubt
Contributor III

I have a TWR-K64F120M board. I can use the OpenSDA connection with the Segger software and everything works fine. When I try to use the on board JTAG connector (J5) with my J-Link probe it fails complaining about the target voltage being too low. I'm powering the board using the OpenSDA mini-USB. Both the OpenSDA and the J-Link probe show up in the device list when I start the J-Link GDB server.

As a sanity check I tried this same set up with a TWR-K21F120M board and it also works fine. I don't know if it means anything but the board was shipped with a plastic clip over the JTAG connector.

ラベル(1)
0 件の賞賛
返信
1 解決策
2,011件の閲覧回数
BlackNight
NXP Employee
NXP Employee
0 件の賞賛
返信
2 返答(返信)
2,012件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Check the jumper settings (J32, J39), see http://mcuoneclipse.com/2014/03/02/first-steps-with-the-freescale-twr-k64f120m/

I hope this helps,

Erich

0 件の賞賛
返信
2,011件の閲覧回数
intractablesubt
Contributor III

Thanks Erich,

J39 was the key. Off for Segger, On for OpenSDA.

0 件の賞賛
返信