TWR-K64F120M and Segger J-Link Probe

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TWR-K64F120M and Segger J-Link Probe

Jump to solution
978 Views
intractablesubt
Contributor III

I have a TWR-K64F120M board. I can use the OpenSDA connection with the Segger software and everything works fine. When I try to use the on board JTAG connector (J5) with my J-Link probe it fails complaining about the target voltage being too low. I'm powering the board using the OpenSDA mini-USB. Both the OpenSDA and the J-Link probe show up in the device list when I start the J-Link GDB server.

As a sanity check I tried this same set up with a TWR-K21F120M board and it also works fine. I don't know if it means anything but the board was shipped with a plastic clip over the JTAG connector.

Labels (1)
0 Kudos
Reply
1 Solution
743 Views
BlackNight
NXP Employee
NXP Employee
0 Kudos
Reply
2 Replies
744 Views
BlackNight
NXP Employee
NXP Employee

Check the jumper settings (J32, J39), see http://mcuoneclipse.com/2014/03/02/first-steps-with-the-freescale-twr-k64f120m/

I hope this helps,

Erich

0 Kudos
Reply
743 Views
intractablesubt
Contributor III

Thanks Erich,

J39 was the key. Off for Segger, On for OpenSDA.

0 Kudos
Reply