TSS library does not scan multiple keypads in kds

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

TSS library does not scan multiple keypads in kds

1,157 次查看
gustavoparlanti
Contributor I

Hi have a project in KDS using the TSS library and now I can compile without any error and I can detect one key interrupt, I have 6 keys and only one key perform the callback, it seems that the scan does not work.

I did the same proyect in CW 10.6 and works perfect. I could not find which is the issue in KDS and I have the same configuration into the PE TSS component.

I attach the project for KDS

Original Attachment has been moved to: K60_Panel_Test.rar

标签 (1)
0 项奖励
回复
2 回复数

1,061 次查看
gustavoparlanti
Contributor I

Hi Alice

Yes it is a custom board, and all electrode works well,

I have the same project in CW 10.6 and the board works perfectly, but now we want to migrate to KDS and just only work one key, not the others and if I change the electrode pin into the component I verified that all electrodes works in KDS but not all together, it seem that the scan function it is not working or something like that. Any help or idea are welcome.

Gustavo.

0 项奖励
回复

1,061 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Gustavo,

Does your board is customer board ?

I think yes,  so please debug step one by one to to check the statues of TSS channel

when press keys , especially check the difference between one can work well and one can not .

BR

Alice

0 项奖励
回复