Suspended : Signal : SIGTRAP:Trace/breakpoint trap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Suspended : Signal : SIGTRAP:Trace/breakpoint trap

5,821 Views
kayathrim
Fresh Out Contributor

Hi all,

 

I have installed KDS 3.00 IDE. I am importing the KDS3 FSFK project from FreescaleSensorFusionRevision5. After Updating KDS, I am getting error like Suspended signal : SIGTRAP  during debugging. For selecting the device MK22FN1M0Axxx12  need to update the KDS. Is anyone faced the problem.

 

Regards,

Kayathri

Labels (1)
0 Kudos
Reply
2 Replies

4,888 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Kayathri,

At first , i recommend you create one simple project to have a try , if it is the same problem ,

please check the PE driver version on your PC , install the latest one .

If it still can not work ,please uninstalled the PEMicro Eclipse Plug-in from KDS, and re-installed it again .

PE Micro debugging issues with KDS and MKL03 microcontroller

If only the FSFK project can not work ,

What about the system frequency of your project ?

If too low , the P&E can't working well with low frequency, you can use J-link to instead to have a try .

Hope it helps

Alice

0 Kudos
Reply

4,888 Views
kayathrim
Fresh Out Contributor

Hi Alice,

Thank you for your suggestions. I have updated the KDS once again. FSFK project is working now.

Regards,

Kayathri

0 Kudos
Reply