Support for external FLASH memory within the KDS and PE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for external FLASH memory within the KDS and PE

1,229 Views
anilnadargi
Contributor II

Hi ,

 

I need to support external FLASH memory to be configured for m_text ( code ) .

 

How to add driver support and configuration for the same in the KDS IDE using Processor Expert.

 

Thanks in Advance.

Labels (1)
0 Kudos
Reply
1 Reply

1,090 Views
trytohelp
NXP Employee
NXP Employee

Hi Anil,

I recommend you to refer to the post:

    Is it possible to force code into a non-standard section?

Under Build options you can change the memory definition generated by Processor Expert in the dinker file.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply