Support for external FLASH memory within the KDS and PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Support for external FLASH memory within the KDS and PE

802件の閲覧回数
anilnadargi
Contributor II

Hi ,

 

I need to support external FLASH memory to be configured for m_text ( code ) .

 

How to add driver support and configuration for the same in the KDS IDE using Processor Expert.

 

Thanks in Advance.

ラベル(1)
0 件の賞賛
返信
1 返信

663件の閲覧回数
trytohelp
NXP Employee
NXP Employee

Hi Anil,

I recommend you to refer to the post:

    Is it possible to force code into a non-standard section?

Under Build options you can change the memory definition generated by Processor Expert in the dinker file.


Have a great day,
Pascal
Freescale Technical Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信