SDK CDC driver compatibility to Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK CDC driver compatibility to Android

2,249 Views
MAPC
Senior Contributor I

Hello,

 

We are on a new project in which we need to connect several devices to a host. This host can be just a common PC running Windows or a gadget like a tablet or a smartphone running Android.

 

Maybe anybody can answer our question: Is the Freescale KSDK USB CDC driver (fsl_ucwxp.inf) also compatible to Android hosts?

 

If not, is there an alternative solution?

 

 

Thanks and best regards,

 

Marco Coelho

Labels (1)
Tags (3)
0 Kudos
Reply
3 Replies

1,904 Views
ivadorazinova
NXP Employee
NXP Employee

Hi Marco,

please, have you tried it by this way?

mik3y/usb-serial-for-android · GitHub

Best Regards,

Iva

0 Kudos
Reply

1,904 Views
MAPC
Senior Contributor I

Hi, Iva

I saw this driver on Community and we are testing it. We will see if it works very soon.

Thanks and best regards,

Marco Coelho

0 Kudos
Reply

1,904 Views
nishantomar
Contributor I

Hi Guys, 

Was someone able to get the USB driver for android system ?

regards

Nishant

0 Kudos
Reply