Project-file subdir.mk not up to date!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Project-file subdir.mk not up to date!

1,385 次查看
oaf
Contributor IV

Hi,

 

We are using KDS to create libraries which we use on both M4 and M0+, and they all exist in Debug and Release versions.

Today I found that my M4-Debug version (M4-Debug\mmSrc\MMComm\subdir.mk) has more files than the M0-version!!!

It seems that the subdir.mk is only updated on the actual build target?

Is this right or am I missing something?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,161 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

subdir.mk is Automatically-generated file after build.

can you please:

1. manually remove it from your project folder.

2, do "project", "clean..." then rebuild your project. this can generate a new subdir.mk file.

can it work for you?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复