Program "make" not found in PATH on KDS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program "make" not found in PATH on KDS

3,709件の閲覧回数
corydavis
Contributor I

Hey all,

 

I am trying to run a program on the FRDM-K82F, and during the build I am getting "make" not found in PATH.

At the same time I am getting Program "arm-none-eabi-gcc" not found in PATH.

I have researched this same error and have not been able to find anything that works for my IDE.

Does anyone know what is causing these errors?

 

Thanks for any help

ラベル(1)
4 返答(返信)

2,869件の閲覧回数
corydavis
Contributor I

Yes, I am using KDS 3.0.0. I'm not totally sure how to upload it directly to this thread, but here is the dropbox link.

Dropbox - myProject

Thanks, I appreciate the help.

Cory Davis

0 件の賞賛
返信

2,865件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Cory,

I build your project on my side. I got error as attachment

are those the same error message as your side?

then I found these two files Event.c/Event.h not included in the SW package. can you please double check if the project source codes you sent me are intact?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,865件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello,

the default KDS3.2 project tool chain setting is as following:

pastedImage_0.png

was your project developed by KDS 3.x? can you upload your project here thus we can check it directly?

thanks!


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,865件の閲覧回数
cthhk
NXP Employee
NXP Employee

此答案靠谱~

0 件の賞賛
返信